888-777-4647
Lee Spring Limited USA UK Mexico IT GM FR SP IN China
 

Lee Spring
 Lee Spring
Lee Spring
Lee Springs

Search for Lee Spring REDUX Wave Springs

Attribute Name Value Range Units of Measurement
Wire Thickness Wave Springs Specifications
Minimum Hole Diameter
Outside Diameter
Solid Height
Maximum Rod Diameter
  Select a maximum of two of the following:
  Click the check box of the items that you wish to enter. Remember, only two are allowed
   Free Height  ± 
   F1 Load  ±  @ Height   
   F2 Load  ±  @ Height   
   Rate  ± 

  Spring Materials
  17-7 PH Stainless Steel          
  Note: The Range column will default to 10% of the Value column
  

Lee Spring
corner bottom left  corner bottom right
Lee Spring

  ISO 9001 Registered Company      
  Phone: 888-SPRINGS (888-777-4647) • Fax: 888.426.6655 • Email: sales@leespring.com            © Copyright 2018 Lee Spring Company

Compression Coil Springs | Plastic Springs | Wave Springs | Die Springs | Extension Springs | Torsion Springs | Belleville Washers | Custom Springs