Lee Spring Limited UK USA Mexico IT China
   
 

Lee Spring
 Lee Spring
Lee Spring
Lee Springs Learn About Extension Springs
 Lee Spring
Lee Spring

Click Here to view the Materials page.
Click here for Extension Stock Spring Tolerances and Engineering Notes.

Overview: EXTENSION SPRINGS are attached at both ends to other components. When these components move apart, the spring tries to bring them together again. Extension springs absorb and store energy as well as create a resistance to a pulling force. It is initial tension that determines how tightly together an extension spring is coiled. This initial tension can be manipulated to achieve the load requirements of a particular application. Extension Springs are wound to oppose extension. They are often tightly wound in the no-load position and have hooks, eyes, or other interface geometry at the ends to attach to the components they connect. They are frequently used to provide return force to components that extend in the actuated position.

Applications: Applications for extension springs include automotive interiors and exteriors, garage door assemblies, vise-grip pliers, carburetors, trampolines, washing devices, farm machinery, toys as well as thousands of other uses. Extension springs come in a wide array of sizes, from small medical devices to off-road machinery brake springs.

Configurations: Lee Spring's Stock Extension Springs are supplied with full diameter loops (either machine or crossover center) at a random position. Loop openings are approximately one wire diameter and the direction of wind is optional. Lee Stock Extension Springs are available in both Inch and Metric designs. If exact direction of helix is required, Custom Extension Springs can be made to specification. To fit the function of extension springs, a multitude of hook or loop configurations may be specified. Close winding of the body provides initial tension in the spring to help manipulate the load and rate.

types of ends Extension spring ends include threaded inserts, extended twist loops, crossover center loops, hooks, expanded eyes, reduced eyes, rectangular ends and teardrop-shaped ends, which can all be produced to vary in distance from the spring body. At the design stage of Custom Extension Springs, the length of the hooks at each end of the spring can be adjusted in order to precisely obtain the required spring load at any extended position.

Another common type of extension spring is the drawbar spring. In a drawbar, the load is applied at the ends of long steel loops which pass through the spring's center and are hooked around the opposite end, thus compressing the spring upon loading. Drawbar springs are excellent for use in potential overload situations and offer a built-in definite stop that will continue to carry a static load after reaching the maximum extended length. A common application of the drawbar spring is used when supporting a porch swing.

drawbar spring

Key Design Parameters:
Dimensions: Outer Diameter, Inner Diameter, Wire Diameter, Free Length and Extended Length
• The Free Length is the overall length of a spring in the unloaded position.
• The Extended Length is the length at full rated extension.
Spring Rate and Maximum Load
• The Spring Rate is the force per unit spring deflection.
• The Maximum Load is the load at full extension.
Unit of Measure
• Lee Spring's Stock Springs are specified in both English (Imperial) or metric units. Be sure to specify the preferred unit of measure when looking for Stock Springs using Lee Spring's search engines.


Lee Spring
corner bottom left  corner bottom right
Lee Spring
Lee Spring
corner bottom left  corner bottom right
Lee Spring

   ISO 9001 Registered Company No.1 for Product, Service and Delivery Conditions of Sale | Privacy Policy | Terms of Use
  Tel: +44 (0)118 978 1800 • Fax: +44 (0)118 977 4832 • Email: info@leespring.co.uk            © Copyright 2010 Lee Spring Company
[