+44 (0)118 978 1800
Lee Spring Limited UK USA Mexico IT GM FR SP IN China
 

Lee Spring
 Lee Spring
Lee Spring
Lee Springs Lee Spring Blogs
 Lee Spring
Lee Spring

Lee Spring shows wide range of springs and
fasteners at FAST Exhibition

Lee Spring at the FAST Exhibition
http://www.fastenerexhibition.com/

Lee Spring will be exhibiting a selection of fasteners and springs at the FAST Exhibition on Thursday 18 April at the RAF Museum, Cosford.

“Lee Spring has been exhibiting at this event since its inception” says Chris Petts, Managing Director of Lee Spring. “It is a great opportunity to interact with engineers, manufacturers and product designers, and a chance to show a range of the latest springs and fasteners. We are also able to share our complete product range with visitors through our updated catalogue.”

Established in 2005, the FAST (Fastening and Assembly Solutions and Technology) Exhibition is the UK’s only dedicated bonding and assembly exhibition for design engineers, production professionals, senior manufacturing manager and fastener buyers.

Lee Spring extension springs used in First World War aircraft restoration

The FAST Exhibition event is taking place at RAF Museum, Cosford which holds particular relevance for Lee Spring, following involvement in a recent First World War aircraft restoration project for RAF Museum Hendon.

“Lee Spring manufactured a set of extension springs for the restoration of a Sopwith Dolphin, which was a First World War aircraft, now on show at RAF Museum Hendon” explains Chris Petts. “The Lee Spring extension springs were used for the replica Lewis guns on the aircraft. It was a truly unique application and demonstrates how varied the applications of Lee Spring are.”

Lee Spring has around 19,000 stock springs

With around 19,000 stock springs available, including 2000 new metric additions, Lee Spring offers a comprehensive range of springs including compression springs, extension springs, die springs, torsion springs and REDUX™ wave springs as well as  innovative Plastic Composite™ springs and Bantam™ Miniature springs.

To complement the comprehensive catalogue Lee Spring also offers an expert custom spring design service, employing a variety of materials to suit any application specific requirements.

Visitors can speak with Lee Spring specialists at the FAST Exhibition and make appointments in advance by calling +44 (0)118 974 0412.  For more information, or to order a catalogue please visit www.leespring.co.uk or call +44 (0)118 978 1800.
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
Compression Coil Springs | Plastic Springs | Wave Springs | Die Springs | Extension Springs | Torsion Springs | Belleville Washers | Custom Springs